5/22/2014 8:32 PM | |
Posts: 4 Rating: (0) |
hi Experts im install pcs7 v8 update 1 when i want open simatic manager , this error appear. A few times I change win 7 and install pcs7 , but There are still this problem thanks Friends Attachment2.zip (302 Downloads) |
5/24/2014 3:57 PM | |
Joined: 10/20/2009 Last visit: 4/3/2017 Posts: 215 Rating: (12) |
Hi Freep, Please visit below thread its very helpful: /tf/WW/en/Posts/77053 |
Regards, |
|
This contribution was helpful to2 thankful Users |
5/25/2014 1:58 PM | |
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating: (62) |
Hifreep Check if the drive you are installing PCS7 on is "compressed to save disk space" It may be the cause of the error |
Best Regards |
|
This contribution was helpful to1 thankful Users |
5/26/2014 12:34 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (23) |
Try to install the same inside a virtual machine once. If possible on other machine. |
Follow us on