9/26/2008 9:39 PM | |
Posts: 11 Rating:
|
I have a project in s5, with ip246, and one ip281. We need to chane the system but i want to know if we have a direct blocks to convert. Somebody could help me? |
9/26/2008 9:44 PM | |
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating:
|
> Hi Please check the following thread you will find all the information for S5 to S7 Conversion. S5_S7_Conversion Help |
9/27/2008 3:25 AM | |
Joined: 9/27/2006 Last visit: 9/13/2025 Posts: 12408 Rating:
|
Hello hbosquemx; First, since you don't mention the family of S7 controllers you will be using after the conversion, the reply I am giving will be based on S7-300 modules; but info on the S7-400 modules is available on the same link. Basically, the answer to your problem is that you cannot use S5 modules on a S7 rack. If you are planning some full hardware conversion, you should look into removing all traces of the IP2xx modules and associated function blocks in the S5 program before conversion, and selecting appropriate S7 modules to do a similar job in your new program; this would be the easier path, the FM hardware and firmware would be compatible with the new CPU, there would be support for the positionning and counting functions from Siemens (S5 modules are now past support phase) and replacements would be much easier to come by. And they come with their own dedicated S7 functions to ensure their operations with S7-300or S7-400 CPUs. IP246: positioning module could be replaced by: FM 353: positioning module for stepper motors IP281: counter module could be replaced by: FM 350: single-channel fast counter up to 500 kHz FM 350-2: 8-channel counter, up to 20 kHz per channel https://www.automation.siemens.com/simatic/regelsysteme/html_76/produkte/sb-fm357.htm Hope this helps, |
Last edited by: dchartier at: 9/27/2008 3:36 AMLast edited by: dchartier at: 9/27/2008 3:26 AM |
|
9/29/2008 6:35 PM | |
Posts: 11 Rating:
|
Hi I need to change from s5->s7 ip246 &ip280 to fm453 & 450-1, i need to know if siemens have a direct converter thanks |
9/29/2008 6:46 PM | |
Posts: 487 Rating:
|
No. There are no automatic conversion tools available. You will need to do this part manually. |
Follow us on