11/3/2015 3:20 PM | |
Posts: 43 Rating: (0) |
Hello everyone, I have an APL_OP_BUTTON (see picture 1 and 2). When I open this I want to let the user choose between 9 options, which are buttons (APL_OP_BUTTON4) see picture 3. I copied those templates from another PDL. But somehow only 7 buttons are showing up, instead of the 9 button (see picture 3 and 4). Where do I have to search to fix this problem? Can anyone explain this to me, I cannot find a solution in the APL_styleguide. Thanks in advance, Wouter Attachmentimages.rar (425 Downloads) |
Last edited by: wouterdejong at: 11/3/2015 5:31:21 PM |
|
11/4/2015 10:48 AM | |
Posts: 43 Rating: (0) |
Dear Harry, Thanks for the great explanation! I followed those steps, but it looks like my APL_OP_BUTTON doenst update with the lattest script. How do you update the APL_OP_BUTTON's to have the latest APL_InitializeBinaryInputDialog.fct? I compiled the script and it seems to work, but I still dont have the option in my attributes on the APL_OP_BUTTON to change 9 buttons, i can only edit 7 button. And how do you know that I need to use the APL_InitializeBinaryInputDialog.fct for the APL_OP_BUTTON? I added the script in the attachment. AttachmentAPL_InitializeBinaryInputDialog.fct for 9 buttons.txt (491 Downloads) |
Last edited by: wouterdejong at: 11/4/2015 10:53:43 AM |
|
11/4/2015 12:03 PM | |
Joined: 2/21/2014 Last visit: 3/14/2024 Posts: 652 Rating: (345) |
Hi, the properties of button 8 and button 9 will not come automatically in the button. you need to edit this button and add these new properties. in one property "OpAreaPicture" of this button the name of the pdls is mentioned. this tell that in runtime when this button is clicked, that pdl will open. if you open this pdl in graphics designer and check Open picture event, this FCT name is mentioned. it means when this pdl is opened, this script will be called which takes the property value from the button and then sets the properties of the buttons in operation area. for more details see attached pictures. It is a lot to explain, but I tried my best to explain. it seems you script is ok. I would recommend that you make a copy of original fct and pdl and rename it. use the new one in you faceplates and keep the originals as it is so that your changes will not affect other things.. I hope I could help you. Thanks, HarrY Attachmentimages.zip (408 Downloads) |
Last edited by: HarrY ji at: 11/4/2015 12:04:18 PMLast edited by: HarrY ji at: 11/4/2015 12:06:07 PMYou can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
This contribution was helpful to1 thankful Users |
11/4/2015 1:41 PM | |
Posts: 43 Rating: (0) |
Hello Harry, I tried changing it to 7, and then it only shows 7 buttons and not 9, I also checked my permissions and the BinPermBitIndex's are on 0, but this shouldnt matter, right? I send my button pdl in the attachment. Thanks again for helping me out! EDIT: I put the wrong attachment, I edited this on 4-11 13:47 Also it looks like it doenst create the `stBinText8` `stBinLinkText8` `IOLink8` `IOAuthLevel8` and 9 in the Objects tab in the configuration dialog of the APL_OP_BURRON4's in the @PG_APL_OA_Binary107.pdl Attachment@PG_Tankdata_Standard.rar (402 Downloads) |
Last edited by: wouterdejong at: 11/4/2015 1:46:48 PMLast edited by: wouterdejong at: 11/4/2015 1:47:20 PMLast edited by: wouterdejong at: 11/4/2015 3:17:41 PM |
|
11/4/2015 3:27 PM | |
Joined: 2/21/2014 Last visit: 3/14/2024 Posts: 652 Rating: (345) |
Hi, My mistake I missed to mention one more script to be updated in the same way: APL_UpdateElementOperation.fct should also be updated to include permissions for button 8 and 9
I attach the button which works for me. I just took your button and updated few things. I added the permission BinPermBitIndex8, BinPerm2BitIndex8, BadQCBinLink8. do it for 9 also please note: all the new properties should have proper name similar to the names of already exisiting properties for buttons 1-7.
I hope this helps. it works for me now. you need to connect the proper tags.
Harry
Attachmentbutton.zip (411 Downloads) |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
This contribution was helpful to1 thankful Users |
11/5/2015 9:50 AM | |
Posts: 43 Rating: (0) |
Hello Harry, Thanks for all this help. I send some printscreens and code files in the attachment, maybe you can find what is wrong with it. Thanks in advance EDIT: fixed it, authorization problem AttachmentPrintscreens and tekst file.rar (387 Downloads) |
Last edited by: wouterdejong at: 11/5/2015 11:13:37 AM |
|
Follow us on