6/29/2013 8:40 PM | |||
Posts: 55 Rating: (0) |
hello i have one s7 1200
but 1-on hmi i put some touch on-off soft,i connected tag,but when i run plc,not work,practicaly,i need from hmi when i touch the switch,to on-of one output [schnippschnapp]i am in italy,and i talked this week more times with siemens office milano,italy,,they told me ,,i call you back,but nothing,they not respond thanks AttachmentDIGITAL+ANALOG1.zip (615 Downloads) |
||
Last edited by: O_Moderator at: 6/30/2013 8:31 PMsecond question is splitted to /tf/WW/en/Posts/93877#top |
|||
6/29/2013 9:39 PM | |||
Joined: 1/28/2009 Last visit: 10/6/2024 Posts: 6849 Rating: (1365) |
Hello, Please provide snapshots of the button you have problem with.It is normal to define tags in "event" properties of button,But as shown in the attachmnet there is no action defined for selected button.[schnippschnapp] Best regards Hamid Hosseini Attachmentbutton.zip (826 Downloads) |
||
Last edited by: O_Moderator at: 6/30/2013 8:36 PM |
|||
6/30/2013 9:32 AM | |
Joined: 1/28/2009 Last visit: 10/6/2024 Posts: 6849 Rating: (1365) |
Hello AutoGen_667937, There are lots of issues discussed in this thread and even a wrong selected conference.I can only help you about the "button" and a bit in PID issue.For the button issue, please follow what I have done:
Best regards Hamid Hosseini Attachment1200_button.zip (647 Downloads) |
6/30/2013 11:42 AM | |
Posts: 55 Rating: (0) |
cable lan,plc-switch(tp-link 1gb)-hmi-computer when i go in networking devices,i can see,plc communicate using profinet with hmi,i have connection i can go online,fo test my hw switch PHYSICALand work ,i can on-off all out,Q0..Q4,using I0.0....I0.5, i connected and write event,for modify bit,in hmi,each button on-off, i put bit for on and reset for off when i dont have connection between plc and hmi,from hmi the button,remain on but when i connect with plc,no,work just with phisical switch,i cant understand where is something wrong can you help me? thanks |
6/30/2013 11:53 AM | |
Joined: 1/28/2009 Last visit: 10/6/2024 Posts: 6849 Rating: (1365) |
Hello, In your original project there was no connection defined between the PLC and HMI.Check as attachment.The procedure is simple, just add HMI to same network in "network view" or "device configuration". Best regards Hamid Hosseini AttachmentNETWORK_CONNECTION.zip (679 Downloads) |
Last edited by: hdhosseini at: 6/30/2013 11:54 AMLast edited by: hdhosseini at: 6/30/2013 11:54 AM |
|
6/30/2013 12:11 PM | |
Joined: 1/28/2012 Last visit: 7/23/2024 Posts: 519 Rating: (83) |
I have little doubt that your PLC is not communicating with HMI. . |
Regards, |
|
6/30/2013 12:26 PM | |
Posts: 55 Rating: (0) |
and i have some dubt but i connected and plc with hmi directly,with cable ln direct or crossover,nothing changed,so.......
|
6/30/2013 12:53 PM | |
Joined: 4/17/2012 Last visit: 8/30/2024 Posts: 474 Rating: (10) |
Hi, Give your HMI screenshot after configure all the connection as per network connection pdf
|
Follow us on