2/22/2018 11:15 AM | |
Joined: 2/5/2013 Last visit: 3/26/2024 Posts: 287 Rating: (5) |
Dear Sirs, I've added a discrete alarm with a custom text and value from a tag, it works fine but in log I find both incoming and outgoing event, is there a way to log only the incoming event for an alarm? I need to register only variation from 0 to 1 not 1 to 0 is there a way to disable the outgoing status to be logged to file? Thanks, BR ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/22/2018 3:21:52 PMNew subject after splitting |
|
2/23/2018 8:41 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hey summer, you can make different alarm classes. In the settings of the alarm class you can activate/deactivate archiving! For archive tags you can define a deadband for logging under the Settings of the tag. With best regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|