6/24/2015 7:12 PM | |
Posts: 70 Rating: (1) |
Hi jacek, I'm using the 0.25 as the min value for the Scale_X fucntion. Thanks for the help |
6/25/2015 7:47 PM | |
Posts: 70 Rating: (1) |
Hi, Yes, I am using the ID1000:P (I do not know if I should be using the ":P" but I read in the forum that it allows the immediate reading). However, the value of this variable that appears in the HMI (I put it as you suggested) is 0. I also changed the HSC from frequency to counts and even then the value of the "ID1000:P" is 0. This means that is probably some configuration problem, is it not? The screen shoots that you asked are in the attachment. Thank you for all the help that you have been giving me AttachmentCaudalimetro.rar (110 Downloads) |
Last edited by: Min_Moderator at: 6/26/2015 10:22:18 AMRename attachment |
|
Follow us on