3/19/2024 6:53 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, As you already mentioned, the Update Collection is just a bundle of updates. It is easy to use since the installer only installs the updates for the already installed components. I also have experience with installing separate updates, which is just more effort if you need several components to be updated. But sometimes it is conventient. For example when you need to have a CFC update, you can just install the separate update on the ES and you won't have to touch the OS servers and clients. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |