2/10/2020 2:34 PM | |
Posts: 8 Rating: (1) |
Hello all, I have VMWare Wrokstation 15.5 running a VM of Windows 10 64bit. In the VM I have TIA portal V16 and PLCSim Advance V3.0. PLCSim Advanced is setup for distributed networking. I have started up a PLC in PLCSim Advanced from TIA Portal and gone online. It is working well and I can connect to the web console from the VM. From the VM I can ping the simulated PLC and I can ping the host machine. From the host machine I can ping the VM IP address but I cannot ping the simulated PLC. The firewalls are disabled on the guest machine (all three profiles). From the host machine Proneta can see the guest VM, but not the simulated PLC. Why can I not ping the PLC from the host machine? Imgur link that shows all of my screenshots. [snip] AttachmentScreenshots.zip (1028 Downloads) |
Last edited by: UselessChimp at: 02/10/2020 14:34:56Last edited by: Jen_Moderator at: 02/11/2020 09:45:38Removed links and added files as an attachment. |
|
This contribution was helpful to2 thankful Users |
2/10/2020 2:45 PM | |
Joined: 5/12/2006 Last visit: 9/27/2024 Posts: 22376 Rating: (3015)
|
Hi, for what you use Gateway 192.168.0.1? Christoph |
2/19/2020 1:36 PM | |
Joined: 8/3/2009 Last visit: 9/27/2024 Posts: 13803 Rating: (1741) |
Hello perhaps its only a handling issue of the VM Ware... If you have a Workstation Pro then you can check : https://www.youtube.com/watch?v=AGeIJzrZpck Bye Murof |
Last edited by: Jen_Moderator at: 02/20/2020 10:52:56Embedded video. If this Information really helps, you could use the Rate function |
|
5/14/2020 8:15 PM | |
Posts: 1 Rating: (0) |
I have also the same problem :( I hope we receive soon an answer about the solution. |
Follow us on