9/3/2020 8:39 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, Small changes can be downloaded without stopping runtime on the server. A simple change of unit is possible with a change only. There are some restrictions such as a full OS compile, which requires a full download. The following situations require a full OS download:
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
9/4/2020 3:04 PM | |
Joined: 11/28/2019 Last visit: 3/24/2024 Posts: 20 Rating: (0) |
AAh ok good. Thank you very much for this information. |