10/27/2017 8:36 AM | |
Joined: 8/3/2009 Last visit: 6/14/2024 Posts: 13030 Rating:
|
Hello RG82 We work also with SmartServer and Comfort Panels. The TP700 Comfort supports up to 3 Smartclient connections at the same time. So yes it is possible to access the Panels from a PC and at the same time from a Smart Client app from Mobile Phone. At our local network it works without problems. Do you have tested it in local network also? if it works here then the function is basically OK. Then the only Problem should be the network connection and Ports from "outside". Do you try to do a ping from Mobile Phone to the Panel? or from the Panel to the Mobile Phones IP? (For Mobile Phones there are apps for ping, and on Panel you can use the commandline) I´m Sure you know this FAQ: https://support.industry.siemens.com/cs/de/en/view/109476153 Bye murof |
If this Information really helps, you could use the Rate function |
|