9/10/2013 9:08 AM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Hello Scotty13, Did you try to perform a factory reset - Resetting to factory settings or thisalternate method. BTW what is the order number of the CPU which you are using. Also mention the firmware version of the CPU. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
9/10/2013 11:41 AM | |
Posts: 19 Rating: (0) |
thx. I only extract MC from PLC and all is working:) |
This contribution was helpful to1 thankful Users |
5/10/2015 3:18 PM | |
Joined: 4/24/2010 Last visit: 9/12/2024 Posts: 16 Rating: (0) |
Im in same problem How to do "extract MMC from PLC"like you said |
8/26/2015 8:53 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by plctoan is split to a separate thread with the subject V13 SP1, loading the hardware configuration failed ( 0020-32 20 ). Best regards |
10/6/2015 11:25 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by thanhbk2001 is split to a separate thread with the subject Error when Compiling Configuration of PLC S7-1200 on TIAportal V13 SP1. Best regards |
Follow us on