12/4/2009 11:20 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Testermax , in add what Nil96said, need make some changes in HW config os actual PC Station: now setted up with ES HW and need modify with OS Server HW (computer name, IP address, MAC address and so on) in according with PCS7 Server/Client configuration. Then add in project all client PC station as well as Nil96 said. Remeber to update license, OS Server License needed Reagrds |
12/4/2009 1:24 PM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Testermax, I guess you are using Win Xp for actual ES/OS project. Instead need W2K3 for server station, and keep your ES station as well ES only or OS client as you like. The question is you need new phisical PC for server, and need configure new "PC Station" in HW configuration. I suggest you to change your actual configuration in "PC Station" as well as Nil said before, just remeber to change everything (station name, IP/MAC address and so on...) when done, go ahead with others configuration (PC station clients) P.S.: remeber you need right license for servers and clients Regards |
This contribution was helpful to1 thankful Users |
12/23/2009 8:52 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Testermax, |
1/4/2010 3:29 PM | |
Posts: 159 Rating: (3) |
Hi CBo and Happy new year to you!
Do you think it would be better to cut/paste ES_OS station and change it to an OS server, in an OS server subproject (and not just cut/paste the OS(1) object from the ES_OS pc station)? The link above "What should you do ..." doesnt seem to point to the right place... But your point, "to clean your original ES_OS project from runtime data" caught my attention! Can you explain why this is important? |
1/8/2010 8:26 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Testermax , |
This contribution was helpful to1 thankful Users |