11/11/2013 6:33 PM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
Hello, I have some problems with the PCS7 8.0 SP1 version. Opening CFC charts is very slow...takes about 8-10 seconds to open a CFC chart. Opening WinCC explorer or starting up Simatic manager is quickly... It only responds slow when using CFC... What could be the reason? My hardware: Asus Intelcore i7-2670QM (4 cores i believe) 2.20gHz 8 gb installed memory 64 bit Windows 7 Ultimate SP1 PCS7 8.0 SP1 Page file is set to 11952mb... PCS7 was installed when page file was set to 12000mb, I changed it already to "system checks page file automatically" and tried setting it to 16000mb. No change It is a clean windows installation, installed my McAfee antivirus enterprise 8.8 and third party software such as malwarebytes etc.. After that installed PCS7... Can somebody give me some pointers? Thxxx |
If I could help you, you can use the RATE button. Thank you. |
|
11/12/2013 12:54 AM | |
Posts: 2661 Rating: (279)
|
Hi Orcea, Have you verified if this is project specific or in general the CFC editor is slow? What about other editors? Regards |
11/12/2013 7:28 AM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
Hello Phantom, I checked two other projects and it was the same. I'm retrieving the projects on D partition, so I tried to retrieve on C partition. Same response... Just last night, I opened the APL_EU example (with the APC examples) and all those charts opened within 4 seconds, instead of 8 Doesnt matter it is a CFC, Control Module or Process Tag Type The rest of the editors seems ok..As I mentioned, WinCC explorer opened quickly, same as Graphics designer, EDIT: I just retrieved a project made with v7.1 migrated quickly to 8.0 sp1 and those charts open like a charm!, I made a new project with the wizard and those charts are opening slow.... |
Last edited by: Oreca at: 11/12/2013 7:51 AMLast edited by: Oreca at: 11/12/2013 7:42 AMIf I could help you, you can use the RATE button. Thank you. |
|
11/13/2013 12:20 PM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
hmm, i checked the error logs, but no errors...Also I checked the databases that are created for the project and checked this with the example project and new project but no differences in memory allocation etc... Still strange that the example project opens charts fast, but every new project created is twice as long... I reinstalled PCS7 8.0 sp1 but nog change |
Last edited by: Oreca at: 11/13/2013 12:21 PMIf I could help you, you can use the RATE button. Thank you. |
|
11/13/2013 1:40 PM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
Update: The problem lies within the multiproject. Goes for all multiprojects I removed AS project for editing, and the charts are opening fast. The APL example is also a project, not a multiproject... Maybe someone know where to look next? |
Last edited by: Oreca at: 11/13/2013 7:21 PMIf I could help you, you can use the RATE button. Thank you. |
|
1/16/2014 7:24 AM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
Hello Peet Sounds like the same problem!! Also that the VMware is working fast, which is the same setup as my "real" laptop. I remember having PCS7 7.1 with no problem at all.. Anyway, since the last update--> PCS7 8.0 SP1 update 1, the opening of CFC is a bit faster ...You can try to update the system. I have no solution, tried a lot also checking SQL databases, increasing memory of database, but no change at all.... Very annoying |
If I could help you, you can use the RATE button. Thank you. |
|
5/13/2014 4:04 PM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
Hello, perhaps this FAQWhat can cause the start of SIMATIC PCS 7 applications being delayed? is helpful for you... Regards jumo |
This contribution was helpful to1 thankful Users |
5/15/2014 12:31 PM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
Hello Jumo, I will check this out, maybe in there is a solution Thx for the feedback! |
If I could help you, you can use the RATE button. Thank you. |
|
8/4/2014 11:38 AM | |
Posts: 62 Rating: (2) |
Hi, I have the same problem. We found out that after not set 'master library', CFC editor seems to work faster. Hope this may help. :) |
9/24/2014 2:00 PM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
Hello Yuwanee, It indeed works with me when removing the master library. Today I installed PCS7 8.0 SP2 and the opening of charts is fast as it should be WITH a master library. Problem seems to be solved in SP2. What it was I dunno, but I love it |
If I could help you, you can use the RATE button. Thank you. |
|
9/24/2014 3:37 PM | |
Posts: 5 Rating: (0) |
Yes, after instalation SP2, it works like charm. Hopefully will not be the same problem in PCS7 version 8.1, which will be released soon. |
5/24/2018 12:30 PM | |
Joined: 6/19/2017 Last visit: 5/29/2024 Posts: 8120 Rating: (165) |
New question published by mujahid143 is split to a separate thread with the subject where is the exact location of these .alarm logs?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on