8/26/2013 6:26 AM | |
Joined: 7/19/2013 Last visit: 5/15/2024 Posts: 68 Rating:
|
Hi JOTST, I installed Storage Plus in completely new Win XP SP3 and now the old problem doesn't appear again. I started to use Storage Plus following the manual but I can't see the archived segment (.mdf) under my D:\ProgramFiles\Siemens\StoragePlus\Archives Also in View Editor when I browse for a tag, I can't see any tags. My current condition is: In WinCC project PC (host PC) 1. WinCC RT is already running and there are many tag logging there 2. I'm using PLCSIM here 3. TagLoggingFast and Slow are already configured to backup the data to Storage Plus PC 4. The Storage Plus ArchiveDir shared folder already can be accessed from this PC In Storage Plus PC (VM machine connected to host by VMNet1 in the same PC) 1. When I started the StoragePlus Management Console. there is no error in Application Log and Activity Log (empty list) 2. Storage Plus Server services is already running 3. Can't browse any tags which must be received from host PC (WinCC project PC) 4. There is no MDF file under D:\ProgramFiles\Siemens\StoragePlus\Archives Please see my attachment, maybe I missed some procedure Many thanks to you.. AttachmentSP.zip (117 Downloads) |
8/30/2013 4:55 AM | |
Joined: 7/19/2013 Last visit: 5/15/2024 Posts: 68 Rating:
|
Hi JOTST, Thanks for your help..After I changed time segment change to January 01,13. Now looks like the archiving is working, because I can see under my D:\Program Files\Siemens\StoragePlus\Archive there are *.mdf files. But these files gone after a while, is it normal? But when I would like to see Tag Table, Trending, etc I can't see them although I can browse all my archive tags on View Editor and Web Viewer also. My Storage Plus PC name is SINERGI, and my WinCC PC name is ENGINEER. When I browse with server SINERGI in my SP PC I can't see any tags. I only can see the tags under ENGINEER server. I think I nearly there, but still need some guidance from your expert sir. Thx a lot.. AttachmentPicture_SP.zip (162 Downloads) |
9/13/2013 2:03 PM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating:
|
new question published by edsel linis split to a seperate thread with the subject when you use storage plus, is it possible to monitor the trend and value of the archived data on the Operator Station? |
My Forum is the place to personalize your profile, |
|
Follow us on