9/19/2022 12:42 PM | |
Joined: 1/26/2019 Last visit: 8/9/2024 Posts: 4 Rating: (0) |
hello im also having this problem, ive tried syncing the clocks and they update the time correctly, are we sure that the ca is the one found in the lsc res file, becaus in the lsc online settings> certificate settings it asks for a .lcu not a .crt it also wont alow you to update the logo root certificate with the .crt file. fyi...did anyone else notice the exploit to bypass the pasword by just entering the wrong pasword into the cmr and then accesing the logo through the lsc edit: seing as ive bean moved i`ll re-ask my quest. im trying to conect a logo to aws cloud through a cmr2020. when i conect the logo through my pc`s internet everything works perfectly. when i try to conect through the cmr i get the folowing error mesage by sms: ERROR Secure connection to logo! BM 8.3 or higher cannot be established, verification of BM certificate failed i sync the logo clock by seting it to ntp client and the cmr to forword the time of day to logo, time is updated on the logo, however it seams that ther is a lag in the time. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/20/2022 07:03:45New subject after splitting Last edited by: Mo333ritz at: 09/21/2022 07:30:58 |
|
9/21/2022 8:03 AM | |
Joined: 1/26/2019 Last visit: 8/9/2024 Posts: 4 Rating: (0) |
this is what it looks like when im connected |
9/21/2022 11:15 AM | |
Joined: 5/30/2022 Last visit: 9/24/2024 Posts: 582 Rating: (96) |
Hi Mo333ritz, Refence of the LOGO!? Version of LOGO!Soft Comfort? |
If this information really helps, you could use the Rate function. |
|
9/21/2022 11:58 AM | |
Joined: 1/26/2019 Last visit: 8/9/2024 Posts: 4 Rating: (0) |
hi hazard, the logo is a 6ed1 052-1md08-0ba1 fw v1.83.01 and the software is v 8.3 |
Follow us on