2/2/2010 4:23 PM | |
Joined: 5/28/2008 Last visit: 5/23/2024 Posts: 1343 Rating: (141) |
Of course it is possible. one solution can be to create different alarm window. Every alarm window get a bit as symbolic address. The F-Keys also have symbolic addresses. Now, in your program, you have to set the bit of the alarm window if the bit of F-Key is set. For better unterstanding have a look to the program of this application. It is only an example: https://support.automation.siemens.com/WW/llisapi.dll/csfetch/27058037/Set27_S7-200_V1D0_en.zip?func=cslib.csFetch&nodeid=28309772 |