3/20/2007 4:43 PM | |
Posts: 5822 Rating: (412) |
Please... not too hard... Best regards J_Bell |
5/7/2007 9:43 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, If there is/are CDs for Softnet they should be named Simatic Net, speaking about confusing terms. On that PC (without STEP7) is a Simatic Net/Softnet install necessary because of the PG/PC-interface and more of course. See also the FAQ Which license do you need for communication via TCP/IP withWinCC V6.0 SP3? This stuff happened to be confusing because there are that many options and possibillities. Also the WinCC development started before e.g. network communication was not that common as it is now. Let's hope that the WinCC succesor (still under development) is easier to use/understand. |
Smurf |
|
Follow us on