8/24/2010 9:54 AM | |
Joined: 8/31/2005 Last visit: 7/18/2024 Posts: 2198 Rating:
|
Please check if there is a small switch on a side of the memory card. If yes, switch to the other position (en- anddisable write protection, you must set it to no write protection)
The COM settings should be ok, because the error panels can be read. Do you have a orginal SIMATIC TDC memory card with a Siemens lable, or a "compatible" memory card? |
Last edited by: miami at: 8/24/2010 10:01 AMLast edited by: miami at: 8/24/2010 9:54 AM |
|
8/24/2010 12:09 PM | |
Joined: 8/25/2006 Last visit: 8/15/2024 Posts: 2208 Rating:
|
The best solution in such case is OmniDriveLF. This is very useful device for first-time loading. |
Follow us on