12/21/2010 7:34 AM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
GOOD MORNING SIR I WANT TO CREATE THE fbamax.a LIBRARY FILE FOR SOME BLOCKS WITH THE HELP OF D7 FB.GENERATOR V2.1 CAN I CREATE IS THIS POSSIBLE (see attached snaps)...???? HOW CAN I CREATE LIBRARY FILE WITH D7 FB.GENERATOR SOFTWARE FOR EXISTING 19 FUNCTION BLOCKS...??? SIR THERE ARE 19 FUNCTION BLOCK WHICH HAVE NOT fbamax.a FILE (see in attached) WHEN I COMPILE THE CFC PROJECT THIS IS DEMANDING FOR fbamax.a FILE UNFORTUNATELY THIS FILE HAVE NOT IN OUR BACKUP PROJECT.???? THANKS REGARDED AttachmentFB.GEN.zip (269 Downloads) |
MS |
|
Follow us on