9/8/2008 10:32 AM | |
Joined: 8/31/2005 Last visit: 10/22/2024 Posts: 2198 Rating: (328)
|
After installing the Software you can access the FM via routing though the S7-CPU (MPI, PROFIBUS or PROFINET) or directly via a RS232 cable (SC57). With this Software you can generate, modify, download and monitor the FM458 program. For more information look into the getting started: http://support.automation.siemens.com/WW/view/en/14943191 There is a old free DOS-Software that allows tolook inside and change values: http://support.automation.siemens.com/WW/view/en/8806155(choose IBS501) This Software is not released to be used with the FM, in some configurations it works, in some ot. You have to try it. Additonal FM Infos you can find here (butthe most order numbers are old) http://support.automation.siemens.com/WW/view/en/8786707 |
|
|
9/8/2008 10:38 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Hello miami, take your stars from me. Excellent, perfect... answer. best regards P.S. Sorry for offtopic. |
Follow us on