5/7/2008 8:32 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Dear All
I am converting an existing FM458 project so as to replace and old FM458 ( with FEPROM )
with a new FM458 ( with MMC ).
I have the existing software backup, however it seems to be in an older version of S7 sys.
I have updated the libraries however when I compile / do consistency check of the FM 458
software, it is asking for two more libraries : fbabas.a and fbasea.a.
What are these libraries, I cannot locate these in D7 sys folder.
The Consistency check error msg is attached for reference
Can anyone pl guide me on this ?
Regards
Navnag
AttachmentFM458_Error.PDF (475 Downloads) |
There is no such thing as the last bug in a program |
|
Follow us on