4/6/2024 2:33 AM | |
Joined: 12/18/2014 Last visit: 5/15/2024 Posts: 33033 Rating: (4082)
|
What kind of encoder is this? What speed are we talking about? |
4/7/2024 11:17 AM | |
Joined: 1/9/2022 Last visit: 4/8/2024 Posts: 29 Rating: (0) |
encoder resolution is 100 PR |
4/7/2024 1:18 PM | |
Joined: 6/11/2019 Last visit: 5/13/2024 Posts: 2199 Rating: (98) |
- At 1155 rpm that would be 19.25 ups. - 19.25 and an incremental sensor of 1:100 that would be 1925 pulses per second. - 1925 pulses * 2 seconds sampling frequency = 3850 pulses per 2 seconds. This is possible with the logo.Therefore just set the value P4 from B002 to 100 (see example). Ella_68 AttachmentProgrammplan-3.zip (35 Downloads) |
5/3/2024 4:09 AM | |
Joined: 6/19/2017 Last visit: 5/15/2024 Posts: 8049 Rating: (164) |
New question published by Thien Tam is split to a separate thread with the subject Which input pin can be used to read the high speed pulse signal sent by the encoder?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on