9/17/2024 1:07 PM | |
Joined: 10/30/2018 Last visit: 9/19/2024 Posts: 15 Rating: (0) |
Hi everyone, I'm using the TM 1*24V (6ES7 138-6AA01-0BA0) module. I have 2 S7-1500 CPUs configured as redundant, and an ET200SP as a distributed I/O on a PROFINET connection. When I try to configure the HSC block, in the first parameter section called "Basic Parameters," the TM module doesn't appear to be available for selection. What should I do? I've read the documentation, but I couldn't find a solution. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/17/2024 13:59:40New subject after splitting |
|
9/17/2024 1:36 PM | |
Joined: 9/23/2005 Last visit: 10/18/2024 Posts: 4760 Rating: (727)
|
This can be helpful. |
Regards, |
|
9/18/2024 7:23 AM | |
Joined: 10/30/2018 Last visit: 9/19/2024 Posts: 15 Rating: (0) |
With Upd3 of TIA_V19, the problem is solved... |
This contribution was helpful to1 thankful Users |
Follow us on