(2)| 5/29/2024 1:06 PM | |
|
Joined: 12/3/2019 Last visit: 10/29/2025 Posts: 36 Rating:
|
Hi everyone, After a couple of problems with the balluff IO-Link module BNI PNT-508-105-Z015, I would like to share with you a sollution for a "Undervoltage" error in the module. Here are the project configuration:
Here are the steps on TIA PORTAL that you need to follow in order to solve the undervoltage:
Now you should visually see that the LED on the IO-Link Masters Port 0 (LED for pin 2) should be yellow and you should also see that the UA LED on the sensor-hub should be lit. That's all folks for today. Hope that the information above may help you OBS.: I attached the photos of the project and the steps you must follow AttachmentIO-Link folder.zip (608 Downloads) |
Last edited by: Luh_Days at: 05/30/2024 04:32:03 |
|
This contribution was helpful to
|
|
Follow us on