(0)| 2/13/2025 12:30 PM | |
|
Joined: 5/6/2022 Last visit: 1/14/2026 Posts: 589 Rating:
|
Hi Mosselaar, Based on the information provided from the sources, the code '88' on the display indicates that the status display test is being conducted during the power-on phase. However, the issue with LED H1 being ON red and LED H2 being OFF is not explicitly documented: "SIMATIC Industrial PC SIMATIC Box PC 627B: Status display" Since your box PC does not proceed beyond the initial status display test (code '88') and the LEDs are not in the documented state (both Orange during power-on), it suggests a potential hardware failure or a critical error during the initial power-on self-test (POST). Given that the display remains on code '88' and the LEDs are not in a typical state, it is advisable to perform the following steps: Check Hardware Connections: Ensure all internal components (RAM, CPU, storage devices) are properly seated and connected. Power Cycle: Completely power off the device, wait for a few moments, and then power it back on. If the issue persists, it might be necessary to contact Siemens repair department for further assistance as the problem could be related to a hardware defect or a critical system error that requires professional diagnostic tools. If possible, which it does not appear to be, I would perform a factory reset of the IPC to see if it comes out of this state. |
|
If this Information really helps, you could use the Rate function |
|
| 1/14/2026 9:47 AM | |
|
Joined: 7/30/2024 Last visit: 1/15/2026 Posts: 1193 Rating:
|
New question published by AutoGen_2680851 is split to a separate thread with the subject IPC 847E stuck in boot cycle. Best regards |
Follow us on