(0)| 9/25/2014 2:54 PM | |
|
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
Dear Sir, With using character delay time 1 or 4 and Response time 1000 or 2000 and connected trouble free data trrafic 330ohm resister on both end problem is remain. as mentioned in Modbus Serial Line Protocol and Implementation Guide V1.02 Character time is the total time for all bits that are sent per character. For example, with 1 start bit, 8 data bits, no parity and 2 stop bits at 9600 baud, the total character time is: 11 bits x 1sec/9600 bits = 1.14ms This means the silent interval must be at least: 3.5 x 1.14ms = 4.01 ms Third party slave device mentioned A, B, SCR, terminal for RS485 (not confirm which one is (+) , (-) and 1SI module mentioned (A) - (B)+ PE when i connect cross A with B i am able to right the value like function code slave address etc. after trigger the M120.7 as status of Tx, Rx led lights up with 2Hz. when we write function code 3 then both led's flashing but with other function code (1-2-4-16) Rx led not responding. error #811 not steadly its coming after 1or 3 second and some time after 8 second. we are using FB2 and FB3 RECV and SEND function block with Modbus master configuration please see attached. Regard's AttachmentDesktop.zip (290 Downloads) |
|
MS |
|
Follow us on