(2)| 4/13/2015 5:49 PM | |
|
Posts: 6 Rating:
|
I use SFC51 to read LED status from an S7-400H. I get 30 data records returned. 15 from the Master and 15 from the Standby. The values returned are: I can find Siemens documentation to explain the LED index w#16#01 to w#16#13 here: http://support.automation.siemens.com/WW/view/en/23330722 • W#16#0002: INTF (internal error) • W#16#0003: EXTF (external error) • W#16#0004: RUN • W#16#0005: STOP • W#16#0006: FRCE (force) • W#16#0007: CRST (restart) • W#16#0008: BAF (battery fault/overload, short circuit of battery voltage on bus) • W#16#0009: USR (user-defined) • W#16#000A: USR1 (user-defined) • W#16#000B: BUS1F (bus error interface 1) • W#16#000C: BUS2F (bus error interface 2) • W#16#000D: REDF (redundancy error) • W#16#000E: MSTR (master) • W#16#000F: RACK0 (rack number 0) • W#16#0010: RACK1 (rack number 1) • W#16#0011: RACK2 (rack number 2) • W#16#0012: IFM1F (interface error interface module 1) • W#16#0013: IFM2F (interface error interface module 2) Does anyone know what the LED Index W#16#0015 and W#16#0017 mean? (MAINT? BUS5F?) Thanks in advance, |
This contribution was helpful to
|
|
| 3/17/2017 10:08 AM | |
|
Joined: 3/17/2017 Last visit: 7/16/2025 Posts: 1 Rating:
|
Thank You very much sir. It is very helpful. |
Follow us on