(0)| 3/12/2020 4:19 PM | |
|
Joined: 1/12/2018 Last visit: 6/16/2025 Posts: 3 Rating:
|
I have a similar problem A setup with one PLC (1212C) with 4 ProfiNet devices attached (Servo drives) working OK. Changed to another PLC (1214C) with the same 4 devices, now assigned to new PLC. Old PLC disconnected. Hardware and software configuration downloaded separately. All can be detected in "Accessible devices" with correct IP-adresses and ProfiNet names. But going Online says all four devices are "Not reachable", saying ProfiNet Connection parameters wrong. Help much appreciated... More info: Error when going online or starting the PLC: Error: IO device failure - PNIO configuration error (connection parameter) HW_ID= 271 This is the same, also loading older projects using the same PLC and devices. Same outcome even with Antivirus and Firewall disabled on TIA-PC. ------------------------------------------------------------------------------------------ |
Last edited by: Karstenjq at: 03/13/2020 00:13:07Last edited by: Jen_Moderator at: 03/13/2020 08:07:22New subject after splitting Last edited by: Karstenjq at: 03/13/2020 15:12:37 |
|
Follow us on