3/11/2024 10:07 PM | |
Joined: 3/5/2020 Last visit: 4/23/2024 Posts: 8 Rating: (0) |
Hi, If I want to use a device which has about 1400 bytes of data in each packet, how can I calculate the maximum number of devices I can connect to a single PLC? Lets say the 1518 IO Process Image is 32kBytes, does that mean I can only have 32000/1400 ~ 22 number of devices? Is there a way to expand this number? Is it possible to request process IO within multiple scans? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/12/2024 15:11:23New subject after splitting |
|
3/14/2024 8:44 AM | |
Joined: 3/5/2020 Last visit: 4/23/2024 Posts: 8 Rating: (0) |
Hi Hati, Thanks for your response. I tried to check that: CPU 1518-4 PN/DP MFP Product Information Could you please clarify how to calculate the number of IO that can be connected as a function of process image and data-size per IO?
|
Last edited by: The Helping Hand at: 03/15/2024 09:48:56Last edited by: The Helping Hand at: 03/15/2024 09:49:21Link optimized |
|
Follow us on