2/1/2024 2:41 PM | |
Joined: 7/19/2022 Last visit: 9/13/2024 Posts: 384 Rating: (62) |
Hello Morteza7090, Could you indicate the exact reference of the Namur module? |
If this Information really helps, you could use the Rate function |
|
2/1/2024 4:11 PM | |
Joined: 10/6/2023 Last visit: 5/6/2024 Posts: 7 Rating: (0) |
I want 4 channel digital input Namur type. |
2/2/2024 8:35 AM | |
Joined: 7/19/2022 Last visit: 9/13/2024 Posts: 384 Rating: (62) |
Hello, If you refer to the 4DI NAMUR module (6ES7 131-4RD02-0AB0) it belongs to the ET 200S range, for the ET 200SP you must use the 8DI one (6ES7 131-6TF00-0CA0) |
Last edited by: JBS98 at: 02/02/2024 08:35:33If this Information really helps, you could use the Rate function |
|
2/3/2024 7:50 AM | |
Joined: 10/6/2023 Last visit: 5/6/2024 Posts: 7 Rating: (0) |
Hello, i want 4Di NAMUR module(6DL1 131-6TD00-0HX1), this module is belongs to ET200SP, i have one project sample that use this module (refer to the attached picture) But now i cant add this module |
Follow us on