8/12/2024 4:14 PM | |
Joined: 9/27/2006 Last visit: 9/15/2024 Posts: 12282 Rating: (2683)
|
Hello Jodossantos; The message you posted suggests you open the Details button in your programming screen to find more information on the causes of this failure to dowload. What information does this provide? Downloading a configuration or a program to a Safety PLC with Step 7 requires an additional software, Distributed Safety, do you have it installed on your PC? Pease provide us with a list of the programming software you are using, with details on the version you are using. If your version of Step 7 is v5.5 or higher, follow this link to download a trial version of the latest Distributed Safety version. It is fully functional for 21 days after installation but you will need to purchase an active license after that limit. https://support.industry.siemens.com/cs/ca/en/view/109749290 Hope this helps, Daniel Chartier |
8/16/2024 9:04 AM | |
Joined: 8/30/2021 Last visit: 8/16/2024 Posts: 21 Rating: (0) |
Hi! I'm using Step 7 v5.5+SP4 with the F configuration Pack and distribution safety as well. I tried downloading again and the Details say "Cannot Load SDB2000. The system data cannot be loaded to module CPU 416F-2 (R0/S3) of station 416-2F". In attachments you can find this Details image and also the module information. Thanks. AttachmentScreenshots.zip (71 Downloads) |
8/16/2024 2:37 PM | |
Joined: 9/21/2012 Last visit: 9/16/2024 Posts: 4131 Rating: (463) |
Connect your programming cable to the CPU, not the CP card. |
8/16/2024 4:44 PM | |
Joined: 3/19/2020 Last visit: 8/27/2024 Posts: 33 Rating: (1) |
Kindly check below link. https://support.industry.siemens.com/forum/in/en/posts/download-error-13-4589/120487 |
Follow us on