11/14/2024 11:55 AM | |
Joined: 3/14/2008 Last visit: 11/14/2024 Posts: 2130 Rating: (953)
|
Hi, When you first set the force value to 0.0 and a moment later set MV_ForceOn to false, I think the block will react. I think it's in the block that first the MV_ForceOn is handled and then the value is set and that is not how I would see it. Otherwise you have to use a tracking signal -> MV_TrkOn to set the MV back to 0.0 |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on