2/4/2014 8:37 AM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating:
|
); When doing that, the compiler says "Invalid or missing function type". The OSCAT function doesn't have the SCALED output as default, that's one i tried create, because my call doesn't work. When calling the standard library it does this: SCALE_R (X := "HMI Input".Feed_2_Tool1 // IN: REAL ,I_LO := 0.0 // IN: REAL ,I_HI := 15000.0 // IN: REAL ,O_LO := 0.0 // IN: REAL ,O_HI := 100.0 // IN: REAL ); As you can see, there's no "output" from that one... In the FC, the RET_VAL placed in "Return" is the output, but the block call in SCL doesn't take that with the call.. Please help :) Hello, I hope you remember this thread: Error in Call FC from SCL[code](* @PATH := '/Engineering/signal processing' *) Best regards, Hamid Hosseini |
2/4/2014 8:53 AM | |
Joined: 8/27/2013 Last visit: 8/12/2024 Posts: 36 Rating:
|
Sorry... I didn't remember that |
Follow us on