6/20/2016 6:52 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (193) |
Hello, you can use the code in the following FAQ to check weather you are allowed to create an object (a file) in the passed Directory/file path. If you can't you get a error-bit, which can be used to open the popup. My guess is that if the directory is secured by a password, then you can't create the file object.
I don't have an idea about using a windows password during runtime, however. Maybe you can use the HTML browser control or toggle between the Windows function (password window) and the runtime. |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on