9/8/2016 5:23 PM | |
Joined: 11/2/2007 Last visit: 7/16/2024 Posts: 7 Rating: (2) |
Thanks HarrY ji, that was helpful. Following that tip you gave me I found the parameter needed in SSMOpenFacePlate. This function doesn't have the builtin functionality you described, but can be modified to do the same thing. Both functions (the APL one and the SSM one) end up calling the internal function SSMRTOpenFaceplate. This in turn accepts the position of the faceplate as input parameters. I modified the fct file so that it passes the block icon positions Left and Top to the internal function to open the faceplate over the block icon. There's room for improvement as this shows the faceplate over the block icon, not next to it, and doesn't take into account the position of the block icon resulting in a popup sometimes outside the main window. The call ended up like this:
|
This contribution was helpful to1 thankful Users |
Follow us on