5/4/2018 2:30 PM | |
Joined: 2/16/2018 Last visit: 5/6/2022 Posts: 6 Rating:
|
Hello, I have a small issue with my popup while using a faceplate and udt. I have to use a lot of analog values, and to simplify the creation of hmi screens, i created a faceplate with and UDT as interface. Now when i open the popup, i first set the accoding index of my array(udt) to get the right values from my DB. After that, the event will call the popup. My problem now, is, that whenever i switch from one analog value popup to the next one, all my input parameters are still the same as in the previous opened popup. After the second call of the same popup, i get the actual values. I was now testing this for serveral hours and cannot find a solution. I put some pictures in a pdf for you all to see my issue. I hope you can help me with this. I use TIA V14 SP1 - TP1200 Comfort Panel. Greetings Willi Michels AttachmentUpdate PopUp on Call with faceplate UDT.pdf (299 Downloads) |
Last edited by: AutoGen_5806207 at: 5/7/2018 8:19:52 AMLast edited by: AutoGen_5806207 at: 5/7/2018 8:20:34 AM |
|
5/7/2018 3:22 PM | |
Joined: 2/16/2018 Last visit: 5/6/2022 Posts: 6 Rating:
|
Okay, thank you for explaining what i try to achieve here, that might help others aswell as my explanation was not really good. And because it was bad, same as my screenshots, you could not see, that the values shown in the screenshots, are from a different DB. I simply move the inputs from my HMI-DB to my Global-DB and in the end i move the outputs from my Global DB to my HMI-DB. My Global-DB uses defined variables, whereas my HMI-DB uses the indexes. Therefor my index is still from 0-100. The HMI tags that are named, are not used in the popup. I hope my screenshots are better now. AttachmentUpdate PopUp on Call with faceplate UDT Nr2.pdf (201 Downloads) |
Follow us on