2/27/2021 3:33 AM | |
Joined: 7/1/2020 Last visit: 3/11/2021 Posts: 6 Rating: (0) |
I know the post was quite lengthy but can anyone please provide a hint to any problem described above? |
3/3/2021 5:30 AM | |
Joined: 7/1/2020 Last visit: 3/11/2021 Posts: 6 Rating: (0) |
Hello Sir, Thank you for your feedback and sorry for my late response, the CNC is currently in heavy use despite described problems and not much time for anything else :-) Please see attached CNC_backup.zip, it contains whole CNC backup I made (hopefully properly) when I received the machine and also the DISK_MGZ.SPF file as requested. As far as any other documentation I'm a bit short on it, it's a frustrating topic for me... Please check the attached and let me know if I can clarify anything else, I certainly will try. I really appreciate your help! Best regards, Lubos AttachmentCNC_backup.zip (169 Downloads) |
Last edited by: LubosUlo at: 03/03/2021 05:36:32 |
|
3/4/2021 5:52 AM | |
Joined: 7/1/2020 Last visit: 3/11/2021 Posts: 6 Rating: (0) |
Hello! yes, the file is a mess, right! So far I decoded following M functions: Vacuum pump - M13(ON) M14(OFF) Dust collector - M15(ON) M16(OFF) Dust hood - M27(UP) M28(DOWN) (was also opposite way so it was always crashing when changing the tool and they shipped that like this :-)) Apparently they tested it without the shroud assembled. Cooling sprayer system - M23(ON) M24(OFF) Tool storage - M50(ON - forward) M51(OFF - back) (your assumption is correct) 8 tool holders in the magazine, and yes the program has 20 positions... R161 is "-100" and R103 is "-196.95" - that's another cool thing to have the magazine location stored in user parameters which anyone can overwrite... Anyway I will have to tweak the values slightly as the spindle is not picking the tool really as smooth as I would like but for now I can live with it, just let me know if you are going to change the concept where will be these values stored. For your reference I attached picture of all R variables <>0. I really, really appreciate your help! best regards, Lubos
AttachmentR_param.zip (163 Downloads) |
3/4/2021 10:18 PM | |
Joined: 5/24/2016 Last visit: 10/17/2024 Posts: 356 Rating: (52) |
Hello Ludos. I have not "Rewriten" the macro like I would have done it, "if it works, I am not to mess to much with it" So I have moved the M51 to after the Z axis has moved above the magazine. Please be aware that using this is at your own risk AttachmentDISK_MGZ.zip (182 Downloads) |
Follow us on