11/18/2020 3:28 AM | |
Posts: 62 Rating: (0) |
What's the difference between P840 and P852? 840 turns the drive on and 852 starts rotation is that right? |
11/18/2020 8:56 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating: (797)
|
Hello, you can also check out the following function diagrams in the S120 list manual to see where those parameters take effect in detail. FP 2501 Internal control word (connection of p840/p852 to r898) FP 2610 Sequence controller (r898 is mentioned as STW.xx see footnote <5>) https://support.industry.siemens.com/cs/ww/en/view/109781807 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on