8/5/2014 7:20 AM | |
Posts: 2348 Rating: (264)
|
Yes, it's possible, see jobs 00B1..4. Also you can use SFC59/ Both methods are suitable for both S7-300 and S7-400. |
Last edited by: Aret at: 8/5/2014 7:20 AM |
|
8/7/2014 11:17 AM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating: (14) |
I am still not succesful with the diagnostics of the IO modules on the rack.. I want to read the diagnostic data from all IO modules on tha rack continously in OB1. I found some example of reading diagnostic data only in case of faulty module (reading in OB82). I have attached three pictures: 1)Hwconfig.png - my HW configuration. There are I modules, Q modules, Power modules... 2)DiagRead.png - example of implemented program. Fot the test I want to read 10 data records from the first modules. 3)DiagReadModule.png - example of parameters for analogue input module. There is an information for "Group dagnostic" SZL_ID:W#16#B1 Index: I thought that it is position of the module on the rack. But in thread /tf/WW/en/Posts/26517 I found out that it is diagnostic address. But I am not confused now, I could not see any diagnostic address for IO modules, I can see only for power modules. Thank you for any help. Thanks in advance.
Attachment_Diagnostics.zip (1152 Downloads) |
Georgio |
|
8/18/2014 2:19 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Dear Georgio, Please check the attachment. If not helpful, please reply. Attachmentmod_sts.pdf (1577 Downloads) |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
8/18/2014 2:50 PM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating: (14) |
HiSachinpatke. Thank you for you post, I studied these information from help on SFC51... I tried bothSZL_ID:W#16#B1 andSZL_ID:W#16#B2. I have to study it carefully once again. To this time, the corresponding bits have not suited to my hardware and actual status of this hardware Aretadvised me to use SFC59, but to this time I had no opportunity to test it I still cannot finad more deep information. For example in the .pdf file: in 1st Byte, Bit0 to Bit 3: Module class (CPU, FM, CP, IM, SM).... this is general information, but where can I find out which combination of bits means CPU, SM etc.I tried to find out from catalog information from SM, but without success I will study harder Regards. |
Georgio |
|
8/18/2014 5:45 PM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating: (14) |
HiAret. Thank you for your information. I found what I was looking for Hopefuly I know everything what I need for my application... Regards.
|
Georgio |
|
Follow us on