12/28/2018 6:00 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi zonouzi, First of all, I'm very curious why are you using step7 way to design your program using PCS7? Is there a special reason? I think using this kind of programming destroys the whole PCS7 concept. You know that when you do a full AS compile, the instance datablock changes? So, you are kind of screwed when you use this method multiple times...you need to set the correct datablock names again after each full AS compile. For your questions, see below:
|
If I could help you, you can use the RATE button. Thank you. |
|
1/7/2019 12:31 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello zonouzi, plan-in-plan technology or chart-in-chart technology is a method to inserted a CFC chart into another CFC chart. For more information you can get here. How to use the chart-in-chart technology:
|
1/9/2019 8:04 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello zonouzi,
with your method you will not minimize the size of code (kB) you generate. Even will you generate more code, you alone will minimize the number of DBs in your project with this method. When you want to minimize the size of code (kB) you have to use the blocks with "S" at the end, i. e. VlvS. More information you can get here. Back to your original problem.
1) the dimmed icon is from the memo-function of the APL-block, here you get more information about the memo-function. 2) the X in the group display means that you have locked alarms at the faceplate, but you lock icon is open. You can get more information about the group display and lock alarms here. Both errors indicate that the blockicon has not all variables from the block. But I don't know which variables are missing. With regards |
Last edited by: Heisenberg2 at: 1/9/2019 8:08:01 AM |
|
1/12/2019 5:01 PM | |
Joined: 10/10/2007 Last visit: 8/15/2024 Posts: 46 Rating: (0) |
HelloHeisenberg2, You are right (as always), some needed tags are not generated in Wincc. For example OS-internal variables for Memo, "xxx.#TextPermanent" and "xxx.#StatusPermanent" are not generated, despite of marking the "AUTHOR" attribute of the related DB to start with "AdvLib81", as said in PCS7 Libraries APL Style Guide". Moreover: The given links bring me to the following page. I am wondering if you may point me to the link related to "Memo-Functions" and "Lock/Unlock Messages".
my best regards, |
Last edited by: zonouzi at: 1/12/2019 5:03:48 PMLast edited by: zonouzi at: 1/12/2019 5:04:37 PMLast edited by: zonouzi at: 1/12/2019 5:06:51 PMLast edited by: zonouzi at: 1/12/2019 5:09:58 PMLast edited by: zonouzi at: 1/12/2019 5:16:04 PM |
|
Follow us on