2/28/2018 3:27 PM | |
Posts: 64 Rating: (4) |
Hello! I use next module (just 1st channel, other are disabled) - F-DQ 4x24VDC/2A PM HF (6ES7 136-6DB00-0CA0) V1.0 and can't start this module. Attachmentimages.zip (493 Downloads) |
Last edited by: Jen_Moderator at: 3/1/2018 9:25:44 AMAdded all files as an attachment. |
|
2/28/2018 3:39 PM | |
Posts: 64 Rating: (4) |
Parameters by the defaults (I just inserted module to the project from the library). The compilation is completed without errors and warnings |
3/1/2018 6:10 AM | |
Posts: 64 Rating: (4) |
Can anybody explain why I can receive data from other modules in the rack but can't get data from this one? |
3/5/2018 3:52 PM | |
Posts: 64 Rating: (4) |
So, my result is: after I pressed "identification" I've got "module is unreachable"...... (same time other modules are work properly in this ET station) |
3/5/2018 8:05 PM | |
Joined: 5/6/2010 Last visit: 5/5/2024 Posts: 1965 Rating: (272) |
Hello Cerberus13, here is the link to a manual programming safety where this is explained. regards |
3/6/2018 5:51 AM | |
Posts: 64 Rating: (4) |
How can I do that? (check the firmware version). In the project I can see it in "Properties" but what about module? |
3/6/2018 8:11 AM | |
Posts: 64 Rating: (4) |
I download firmware update for the module Firmware Update for ET 200SP F-DQ 4x 24V/2A DC but I can't open page with "Description" - it's open empty page by the link.... How can I make update for the module? (TIA Portal 14 SP1) |
Last edited by: Jen_Moderator at: 3/12/2018 1:18:21 PMOptimized link. |
|
3/9/2018 5:08 PM | |
Posts: 64 Rating: (4) |
If's "F parameters" |
3/9/2018 5:09 PM | |
Posts: 64 Rating: (4) |
and settings for the 1st channel (I use just first channel) |
3/13/2018 3:11 PM | |
Posts: 64 Rating: (4) |
Hello CaOd, DIAG is blinking with green colour |
Follow us on