3/25/2013 10:47 AM | |
Joined: 6/8/2011 Last visit: 9/16/2022 Posts: 40 Rating: (24) |
Welcome. I found solution for runFULLY virtual WINAC RT into VMWARE 9 for developing and testing enviroment. I have Vmware Workstation 9 and Win7 32 bit guest operating system. At Host WIN7 64 Bit. Let,s go: 1.Create VM at hardware compatibility 9 Version. (1 processor with 2 cores , 1 Ethernet Bridged Network Adapter) 2.In Vmware 9 VMX file You must add this lines (very important): ethernet0.virtualDev = "e1000e" bios440.filename="FUJITSU211_314.ROM" 3.Copy into VM folder file from attachment (ROM FILE). 4.Install WINAC RTX 2010 on OS 5.In station configuration Add in slot IF1 IE General card . If You prompted to install drivers from RTX then accept this. From Guest OS this card was removed. Its normal don,t panic . 6.Then From Step7 set IP addresfrom Menu --->PLC---->Edit Ethernet Node. 7. Load program and use Fully virtualized WINAC. If You Have some problems To set IP from Edit Ethernet Node from STEP7 then You can retrive config from WLD file added into attachment. IP addres is 172.16.1.80. If You have further questions don't hesitate to contact me. Best regards. AttachmentWINACRTX_VM.zip (5543 Downloads) |
This contribution was helpful to13 thankful Users |
4/25/2013 10:51 AM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating: (3) |
Help not work. |
4/25/2013 1:43 PM | |
Joined: 6/8/2011 Last visit: 9/16/2022 Posts: 40 Rating: (24) |
What is your config. more details. |
4/26/2013 11:20 AM | |
Joined: 6/8/2011 Last visit: 9/16/2022 Posts: 40 Rating: (24) |
Welocme. Your config its ok. Enter the WINAC properties and uncheck SPEEDSTEP technology. Probbably SPEEDSTEP is active and preventing to idle state the CPU https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=38616807&query=OBs+error&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW Best regards. |
4/26/2013 6:33 PM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating: (3) |
Removed all install just WinAC 4.6 not reboot but WinLC RTX CPU not possible open.Suggestion ? |
4/27/2013 11:21 AM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating: (3) |
Could you check please if VMware file settings and if i put on correct mode (under virtual machine folder) file ROM.Thanks.Regards.is not HP but DELL.
Attachment2013-04-27_111822.zip (1686 Downloads) |
4/29/2013 9:09 AM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating: (3) |
Don't worry be happy already installed on old laptop.Thanks.Regards. |
4/29/2013 3:30 PM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating: (3) |
??? |
4/29/2013 4:16 PM | |
Joined: 5/19/2007 Last visit: 2/12/2024 Posts: 40 Rating: (3) |
Solve PC internal Local.Thanks.Sorry for the apologyze. |
6/11/2013 5:47 PM | |
Posts: 1 Rating: (0) |
Per your instructions, the setup is done on VMware Workstation 9. I am using VMware Workstation 8. Is that going to work? |
6/24/2013 6:39 AM | |
Joined: 5/17/2010 Last visit: 2/21/2022 Posts: 80 Rating: (1) |
Will this also work with VMWare version 6? |
2/28/2015 5:12 PM | |
Posts: 2 Rating: (0) |
To use the WLD file, put the WINLC_RTX CPU into Stop from the RTX Control Panel and then use the File -> Restore menu option.
|
2/28/2015 5:12 PM | |
Posts: 2 Rating: (0) |
To use the WLD file, put the WINLC_RTX CPU into Stop from the RTX Control Panel and then use the File -> Restore menu option.
|
Follow us on