1/31/2018 9:35 AM | |
Posts: 1368 Rating: (126) |
Hello, in forum there´s often the question, how to read out port or mrp status via program. Now, there is a new entry in Siemens Online Support. With the "LPNDR" block library, you receive function blocks with which you can read various device and status information from a PROFINET device and describe parameters.
https://support.industry.siemens.com/cs/de/en/view/109753067 |
Last edited by: Pittiplatsch at: 3/26/2018 10:34:08 AM |
|
This contribution was helpful to11 thankful Users |
3/8/2018 8:51 AM | |
Posts: 1368 Rating: (126) |
no Sorry, only for TIA and S7-1200/1500. |
This contribution was helpful to1 thankful Users |
4/17/2018 1:45 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819)
|
Hello, maybe RDREC can be used also to obtain some data... |
With best regards... |
|
6/7/2018 1:03 PM | |
Joined: 1/30/2006 Last visit: 5/21/2024 Posts: 310 Rating: (57) |
You can find an example on reading the IP Address out in this Example In STEP 7 V5.5, how do you read out the IP address of the S7-300 CPU in the user program? It's based on reading System Satus Lis (SSL). You can find a list of SSL_ID's in this manual from page 669 SIMATIC System Software for S7-300/400 System and Standard Functions |
BR. Sven |
|
This contribution was helpful to1 thankful Users |
10/10/2022 6:18 AM | |
Joined: 10/10/2022 Last visit: 10/10/2022 Posts: 1 Rating: (0) |
thanks
|
Follow us on