12/21/2023 8:55 AM | |
Joined: 9/13/2023 Last visit: 8/29/2024 Posts: 24 Rating: (0) |
Hi, With s7-1500 I have the same problem i can not activate "Permit access with PUT/GET ..." ! Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/21/2023 12:59:22New subject after splitting |
|
This contribution was helpful to1 thankful Users |
12/21/2023 2:14 PM | |
Joined: 3/11/2019 Last visit: 10/9/2024 Posts: 1586 Rating: (289) |
Hi,
which TIA version is used? If V19 was used, this may be different due to changed security settings. regards sancruz |
Feedback appreciated, please rate |
|
2/26/2024 4:22 AM | |
Joined: 2/7/2021 Last visit: 8/4/2024 Posts: 1 Rating: (0) |
Hello, good day. Make sure you have a subnet assigned to the port where you will connect your device to the network. You can check this information in the following path: CPU/Properties/Profinet Interface [x-] /Ethernet Address...
|
8/20/2024 2:28 PM | |
Joined: 4/20/2010 Last visit: 9/17/2024 Posts: 39 Rating: (5) |
Hello, check this topic : https://support.industry.siemens.com/cs/ww/en/view/109925755 Good luck |
Last edited by: Moderator_Lan at: 08/21/2024 06:36:11link optimized |
|
This contribution was helpful to1 thankful Users |
Follow us on