3/15/2016 6:09 AM | |
Posts: 9 Rating: (0) |
Hi Thank you for all information I'm having difficulty to download Data Logs automatically from S7 1200. I have tried using manual, and I followed the instructions step by step, but it was not successful. What I have been able to do is downloading Data Logs manually from the Web Server, which is not what I need. In a purpose of auto saving Data Logs, I'm using Windows task scheduler. The problem is that there is not any specific URL for my Data Logs to download, and I'm getting: “File operation not permitted- no referrer” error message. I have used “64396156_s7-1200_datalogging_docu_v1d0_en” manual, that described this operation on Windows XP. I have tried the instructions on both Windows XP and Windows 7, using different browsers, but I'm getting the same results either way. Is there any other solution for auto saving Data Logs? The software and Hardware that I'm using are listed below: -PC: Windows 7 (x64) -Software: Step 7 Professional (TIA Portal) v13 SP1 -Siemens Module: CPU 1214C DC/DC/DC (6ES7 214-1AG40-0XB0) ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/15/2016 2:19:27 PMNew subject after splitting |
|
3/16/2016 8:14 PM | |
Posts: 124 Rating: (4) |
why do you want to store automatically? you did not use SD card memory? I think, your Run content is wrong. |
Last edited by: saleh at: 3/17/2016 1:16:19 PM |
|
6/29/2018 8:58 PM | |
Posts: 1 Rating: (0) |
Hey, Were you able to solve your problem? I am having the same doubt, but there is not much information on the topic . Regards |
7/3/2018 9:55 AM | |
Joined: 10/2/2014 Last visit: 8/26/2024 Posts: 88 Rating: (15) |
You can use wGet (which is a Linux tool and a windows adaption exists) to download the data logs automatically by calling wGet with a batch file. http://gnuwin32.sourceforge.net/packages/wget.htm https://www.gnu.org/software/wget/ Batch example:
|
9/28/2024 2:49 PM | |
Joined: 2/10/2023 Last visit: 10/1/2024 Posts: 2 Rating: (0) |
Hi I have wriiten a python code to perform the automatic log download without accessing the webserver. Further if you have several logs you can download multip logs simultaneously. In the following code need to update following information
This code support only http not on https if you need to use on https you have to modify 'curl command' and add 'siemens_ad_secure_session' cookie to the session cookies. BR AttachmentForShare_http.txt (7 Downloads) |
Last edited by: AutoGen_1660377 at: 10/01/2024 06:47:26 |
|
This contribution was helpful to1 thankful Users |
Follow us on