10/30/2024 6:39 AM | |
Joined: 10/30/2024 Last visit: 11/1/2024 Posts: 1 Rating: (0) |
Hi everyone, I have a project connected to a Siemens S7-1500 PLC. Everything was functioning properly until I made some recent changes. Now, some tags are displaying a config error,although many other tags are still reading fine. I’m certain the configuration was correct before these changes. One specific issue I noticed is that I can no longer read any Booleans from DB60. I tried disabling and re-enabling the PLC connection, but this did not resolve the issue. In addition, when accessing the interface, I occasionally encounter a blank screen that either freezes the session or requires a complete restart. I’m using Ignition version 7.6.7for SCADA, and I’m wondering if this could be related to the tag errors or connection issues. Could the white background screen issue indicate a deeper problem with communication between the PLC and Ignition, or perhaps a glitch within the HMI setup? Any insights or suggestions on how to troubleshoot both the config error and the white blank screen problem? |
Last edited by: AutoGen_4511432 at: 11/01/2024 04:14:02 |
|
Follow us on