1/15/2015 12:55 PM | |
Posts: 3 Rating: (0) |
Hello! I'm doing theoscillograph on SIMATIC S7-1500. If I useDataLogWriteinstructionevery 50 msonSIMATIC memory cardafter a start button pressedand it will be stopped by a trigger some time, does it mean that ifan ambient temperature up to 60 °C, at least 100,000 delete/write processes arepossible on the SIMATIC memory card???[like in SIMATIC S7-1500 S7-1500 Automation System.pdf] page 4 So if I start write my records in data log every 50 ms I will do it about ~1,5 hour and after that SIMATIC memory card will be damaged and does not work anymore? What is lifetime ofSIMATIC memory card in this case? From whatSIMATIC memory cardlifetime depend on? And how long I can doDataLogWriteinstructionevery 50 ms onSIMATIC memory card? Thank your for your attention!
---------- New subject after splitting from stored simatic log data in memory card and extract this information |
Last edited by: Min_Moderator at: 1/15/2015 1:57 PMSplitted |
|
1/15/2015 2:11 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on