5/12/2008 3:29 PM | |
Joined: 7/15/2007 Last visit: 8/23/2022 Posts: 8 Rating: (0) |
I have made Copy Ram to Rom on the the following GM150s without having any problems with the following Fnr. N-U321492700003 N-U403492700023 N-U321492700002 N-U321492700004 N-U403492700022 N-U321492700005 However, with this unit Fnr. N-U824492700071 when I copy Ram to Rom, it gives me this error "VECTORMV : Parameter P640[0]:Above the valid values." I had Changed the Value of P640 to 600 A but was also rejected. The motor rated current is 680A. AttachmentDiaryMay12.pdf (843 Downloads) |
5/12/2008 4:33 PM | |
Posts: 23 Rating: (2) |
First make offline , set P640 to the right value , then on line and download , it may works . |
Last edited by: Zcomin at: 5/12/2008 4:36 PM |
|
5/14/2008 7:00 AM | |
Posts: 23 Rating: (2) |
Turn off ,turn on,make factory seting .may works |
Follow us on