6/24/2008 5:01 PM | |
Posts: 739 Rating: (55)
|
Hello, pls have a look into the Parameterlist (http://support.automation.siemens.com/WW/view/en/23708204) F0070 CB setpoint fault Refer to F0001 CauseNo setpoint values from CB (communication board) during telegram off time Diagnosis & Remedy Check CB and communication partner P2014[2] USS telegram off time The telegram failure time defines the time within which a valid telegram must have been received. If a validtelegram is not received within the specified time, the drive inverter outputs fault F0070. P2040 CB telegram off time Defines time after which a fault will be generated (F0070) if no telegram is received via the link And into this FAQ http://support.automation.siemens.com/WW/view/en/22329309 http://support.automation.siemens.com/WW/view/en/25339501 http://support.automation.siemens.com/WW/view/en/12324244 |
2/21/2018 5:43 AM | |
Posts: 1 Rating: (0) |
Drive fault F00700 ,please send the solutions. |