5/9/2018 1:16 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi David, it should work with your CPU and IM151. SIMATIC ET 200S Technological Functions the only thing is, that you have a Modified user data interface with an other and newer IM
hope this helps, regards,
|
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
5/9/2018 10:03 PM | |
Joined: 11/12/2017 Last visit: 2/27/2024 Posts: 174 Rating: (1) |
Hi Mopso, Thank you for your reply. I think it should also work as the 6ES7 138-4DA04-0AB0 module does appear in the hardware configuration under my interface module IM151. Is there any reason or advantage of using the FM 350 or FM351 modules over the 6ES7 138-4DA04-0AB0 for general HSC like my application? Thanks again, David! |
6/15/2018 11:56 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello David, stupid question: but if do this job to the VFD is a problem? Ramp up/down? With STEP 7, how can you control servovalves, frequency converters ... or if you use this? |
Last edited by: Ste39 at: 6/15/2018 12:01:29 PMLast edited by: Ste39 at: 6/15/2018 12:09:50 PMLast edited by: Ste39 at: 6/15/2018 12:12:15 PMLast edited by: Jen_Moderator at: 6/18/2018 10:07:40 AMOptimized link. |
|
This contribution was helpful to1 thankful Users |
6/18/2018 4:58 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello David, function with CPU 314-2 DP also, but I think is not free and is quite old Easy Motion Control V2.0 Now Available - Industry Support Siemens I think this is the new version v2.1: Easy Motion Control - Software for SIMATIC Controllers - Siemens and I'm sorry this software I have never used |
Last edited by: Ste39 at: 6/18/2018 5:01:04 PM |
|
This contribution was helpful to1 thankful Users |
6/19/2018 10:57 PM | |
Joined: 11/12/2017 Last visit: 2/27/2024 Posts: 174 Rating: (1) |
Guys, When creating a data block for the data storage of this 1 count module for ET200S I have a question: -For both the inputs and outputs bytes 0 - 3 and bytes 8 - 11, what data type do I need to create. Do I need to use a DINT (double integer)? -Can I also then just create the rest as bytes with standard 8 bits with BOOL data type? Thanks David. Attachment1 Count ET200S Parameters.pdf (205 Downloads) |
Follow us on